Manufacturers > knitter-switch

knitter-switch

Avnet Abacus is an authorised knitter-switch distributor throughout Europe.

knitter-switch is one of Europe’s leading switch manufacturers. Since its foundation in 1966, the company has remained at the forefront of switch technology and now provides an unrivalled range of switching solutions, from basic toggle types to membranes and tactile switches for today’s complex communications applications. 

Featured Products

VIEW ALL

knitter-switch

CTK Series Capacitive Switches

CTK series switches from knitter-switch come in two models with contact ratings of 0.2A and 1.5A allowing the switches to be used with high powered LED lamps.  

MORE INFORMATION
knitter-switch

DPY 1 CB Push-Button Switches

Knitter-switch, one of Europe’s leading switch manufacturers, introduces a new push-button switch which is not only IP 67 but also shows its high quality in the design.

MORE INFORMATION

Ask an Expert

Have a question? Our regional Product Specialists are on hand to help.

 

Get in touch

Documents & Links